Part Number: TCA9800
Hello team,
I got the questions from the customer. Could you please check and support those?
1: For B-side, no need to add pull up resistor? Both A-side & B-side are 3.3V.
2: After enabling the device, low voltage is not 0V, and should be around 0.2V. Is this correct?
3: The customer is using a 30cm flat cable between the master device and EEPROM.
In this case, generally which current source device should we choose?
aside from the section 10.1, if your team has any comment I would like to inform that to the customer.
4: In the case above, which side should we add TCA980x? Is it better to add the master device side?
Thank you for your support.
Best Regards,
Kazuki Kitajima