This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: How to connect a camera using Maxim GMSL serializer (like MAX96705) to a FPD LINK III deserializer like DS90UB960?

Part Number: DS90UB960-Q1
Other Parts Discussed in Thread: DS90UB933-Q1

How to connect a camera using Maxim GMSL serializer (like MAX96705) to a FPD LINK III deserializer like DS90UB960?

Are the two kinds of interface compatible?

Do you have plan to make them be compatible in the future with Maxim?

If they are not compatible now, can we have some methods like modifying the driver or something else to make them be compatible?

Or can we realizing that if we make a board to convert GMSL to FPDLink III like 96706 + 914?

Multiple questions in one quote, Thanks.