This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVS2200: Do we have similar function IC or better P2P replacement with FPF3380UCX WLCSP 12P OVP

Part Number: TVS2200


Hi team, 

As the title, Do we have similar function IC or better P2P replacement with FPF3380UCX WLCSP 12P OVP?

Thanks

Max

  • Hi Max,

    Welcome to E2E!

    The FPF3380UCX is a load switch with internal ESD protection included. In our portfolio we do not have a P2P compatible device or a load switch in general that has the same level of ESD rating on the pins of the device. Where you looking more into the load switch function of the device, the ESD rating, or do you need both?

    Best regards,

    Andy Robles