Part Number: TCAN337
Hello,
We are using the TCAN337DR chip on for CAN bus communication and utilizing the FAULT and Silent functions.
For testing, we are trying out ways to cause the FAULT to go high with Silent Mode on. I've read that there are 4 ways of causing fault, and one of them is the RXD DTO where the CAN bus itself is stuck on the dominant state for a set amount of time.
We've grounded CAN_L and shorted CAN_H to 5V, but we couldn't get the FAULT line to go high. We are also trying this test with Silent Mode turned off and didn't see a FAULT either.
We are driving that line up as directed on the datasheet.
What are recommended ways to cause a FAULT from a RXD DTO?
Thank you.