Part Number: TUSB1210
Hi,
I'm looking at the timing specs of the device ULPI interface.
Data and Control setup time are only specified as a max value of 6ns, when in output clock mode. There are no minimum value specified.
Why? There must be one, isn't?
I'm more used to work with min setup time than maximum value.
I have noticed that it is also specified in the same way in the ULPI v1.1 spec.
Regards,
Pierre