Part Number: LMH1297
Hello,
I am having troubles trying to read back the EOM data from the LMH1297 chip over SPI as outlined in the programming guide. The chip is set up in EQ mode with data entering on the SDI_IO pin. Upon reading the HEO and VEO registers, only 0s are returned. Also, when reading the EOM matrix, it seems like there are not any signal crossings, which would imply that the EOM is not locking onto the data rate. The interesting thing is that I am successfully passing data through the chip. I also noticed that both the carrier detect and course adaptation bits for SDI_IO was high, but I do not have a reclocker lock. I am assuming the reclocker not having a lock is what is causing the EOM to fail. Any suggestions on how to resolve this issue, or direction for diagnosing this issue would be appreciated.
Thanks!
Austin Keener