This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS33: Single line input

Part Number: SN65LVDS33

Hi

What will happen in case one of the LVDS input line is now disconnected (or the POS [A] or the NEG [B] ) and left floating

while the opposite pin keeps working as usual?

Will the receiver still present the proper value (maybe due to the "Attenuation Network" a floating line will be driven to 3.3V*250K/ (250K + 60K) = 2.66V and thus when the opposite proper signal toggles between 3.3V and 0V the required difference between POS and NEG is kept...??)

If the above is true, when I start feeling and kind of problem due to the disconnect net ?

Thanks

Amnon