Part Number: SN65HVD1780
Other Parts Discussed in Thread: THVD2410
Hi,
Do you have the tolerant data of IEC 61000-4-4?
Best Regards,
Kuramochi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD1780
Other Parts Discussed in Thread: THVD2410
Hi,
Do you have the tolerant data of IEC 61000-4-4?
Best Regards,
Kuramochi
Kuramochi-san,
Unfortunately I do not believe this device was ever evaluated against IEC 61000-4-4 and it was not designed for it. If an application requires both high-voltage DC immunity as well as EFT immunity I would suggest the THVD2410 device instead. It is a newer p2p transceiver that features 70-V tolerance and 4 kV IEC 61000-4-4 rating.
Regards,
Max