This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH947-Q1: 1.1V supply current minimum and typical no video output

Part Number: DS90UH947-Q1


Hi Team,

Is there a minimum spec you can provide for the 947 1.1V current consumption when PDB = L? I see 5mA as typical, but is there a low value it will never go below?

With that, is there any detail you can provide on typical current consumption when PDB = H, but there is not OLDI video input or OLDI clock?

Thank you,

Jared

  • Hi Jared,

    Unfortunately, only the typical and maximum values are available in the device datasheet.

    With respect to the current consumption when PDB = H, the available information may be found in Table 6.5 of the datasheet. 

    Sincerely,

    Bryan Kahler