This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848YB: Ready time , bootstrapped - with no autoneg.

Part Number: DP83848YB

I am going to use the dp83848YB device , 

and i need it to be ready as fast as possible , 

i'm using all the bootstraps needed to configure it to my use case - with no autoneg , 

I need an estimation of the time it will take till the phy is ready to create "link" ( assuming the MAC is ready and the endpoint is also ready)