Hi,
Plan to use DPHY Re-timer SN65DPHY440SS in our design. We are using nVIDIA TX1 module for CSI-2 Sink. Since we are using processor module, we can not place DPHY Re-timer close to nVIDIA processor.
Closest placement is possible between DPHY Re-timer and nVIDIA processor 6 inches. Our camera sensor rate is at 360Mbps.
I would like to know what is max distance between DPHY Re-timer and Processor when MIPI speed at 360 Mbps?
Please suggest required pin configuration VSADJ_CFG0, PRE_CFG1,EQ/SCL, ERC/SDA for 360Mbps rate and 6 inch distance between re-timer and Processor