This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS125DF410: simulation method between DS125DF410SQ/NOPB and DS125DF410SQ/NOPB with AMI model

Part Number: DS125DF410

Hello team,

I have a question about the ibis AMI model of the DS125DF410SQ/NOPB.

I would like to simulate between DS125DF410SQ/NOPB and DS125DF410SQ/NOPB, then get the result.

The package model is defined within the Ibis AMI model.
At Figure 3 in the guide of TI_DS1xxDF410_ADS_Project_Quick_Guide.pdf,  it looks like the AMI model is connected to the package model. But I do not be sure  whether it is good or not.

Would you please advise me how we should connect to simulate between DS125DF410SQ/NOPB and DS125DF410SQ/NOPB? Is the ibis+pkg model configuration the correct model for transmission line simulation, or is it I would like to know if the ibis model alone is the correct configuration.

Your help would be so appreciated.

Best Regards,
Akihisa Tamazaki

  • To simulate from the DS125DF410 Tx to a DS125DF410 Rx your simulation topology should have the following components.

    DS125DF410 Tx (AMI) -> LLP48_PKG ->  Transmission Line or Channel -> LLP_PKG -> 100 Ohm termination -> DS125DF410 Rx (AMI)

    Regards,

    Lee