Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869,
Hello
Please how can I install linux driver on RPi 3+ compute module?
For the driver you have provided source dp83869.c. Also I've found patches from https://lore.kernel.org/patchwork/patch/1148980/
I've found, that drivers are natively in linux kernel 5.5+. I could install on RPi only kernel 5.4 as newest possible.
I've tried to apply patches to RPi kernel sources 4.19.127. I miss here from whitch folder apply patches. Which option add to apply patch. Finelly I could compile and run linux kernel 4.19.127 only without adding dp83869 driver support. When I add driver support in "make menuconfig", then I receive error (bellow image).
Thanks for any help
Best regards
Michael Dvoracek