Part Number: SN65LVDS93A
HI,sir:
Our display screen is a single port LVDS 8bit interface, working at - 40 to 85 ℃, the main board of the customer is RGB 24 bit interface, the main board of the customer has space, we would like to recommend sn65lvds93a to the customer for interface conversion, but there are the following questions for the temperature specification:
① Can sn65lvds93a support the above ambient temperature range? Temperature in IC spec refers to IC surface or ambient temperature?
② What is the ambient temperature of sn65lvds93a during factory test? Is there any margin compared with the data in spec?
③ Does sn65lvds93a have car specification chip?
Thanks~