Part Number: DS280DF810
Hello Team,
My self Naveenchandra from Tejas Networks ltd. I am working on behalf of Signal Integrity team. We are performing the SI analysis of a Chip to Optical transceiver Module interface for one of our high speed products. We are using your Retimer device ( i.e DS280DF810 ) for our product.
Presently we are doing correlating the SI results with lab measurements. But we are not getting the same electrical specs measurements in the lab which we are getting in the SI analysis.
Please see our design inputs for more understanding. Below are the SI Analysis inputs considered during serdes channel simulation:
Data rate 28Gbps with NRZ mode, Stimulus used PRBS 31 pattern.
QSFP28 Optical Module as Transmitter and TI Retimer (DS280DF810) as Receiver.
Our end to end board Channel losses are around just IL(Insertion loss) as 7dB and RL(Return loss) as 20dB.
QSFP source amplitude ranges starting from 600mV to 1070mV. Presently its fixed with between 600mV and 800mV. Also, as of now we are considering no de-emphasis at QSFP transmitter side.
See below are the Results variations from SI to Lab measurements (i.e TI GUI tool).
We kept Auto CTLE and AUTO DFE enabled, VGA as 0 and EQ gain as 1. and we are could get eye densisty is around 600mV. But, we could see only 200mV to 250mV as max amplitude in the TI GUI tool measurement. So, its clearly understood that, there is 350mV to 400mV deviations in the results.
As per our understanding, EQ gain settings are playing crucial role in our simulations. but not in the lab measurements.
We would appreciate you if any one get us the valuable support on this. Also, please let us know if you need any other SI setups and Lab setup are required for your reference.
Thanks,
Naveen