Part Number: DP83TC811S-Q1
Hi team,
Any register in DP83TC811S-Q1 to indicate the link-up status register? Thanks.
Regards,
Dongbao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83TC811S-Q1
Hi team,
Any register in DP83TC811S-Q1 to indicate the link-up status register? Thanks.
Regards,
Dongbao
Hi Dongbao,
Register 0x01 bit [2] will indicate link status of the PHY. Please note that you will need to read it twice.
-Regards
Aniruddha
Hi Aniruddha,
Thanks for your reply.
Sorry for the confuse of my question, what i am trying to ask is the MAC-PHY link up register.
Dongbao
Hi Dongbao,
There are no dedicated link up registers for MAC-PHY connection. However, in SGMII mode the is a SGMII Autonegotiation complete register bit that will inform the MAC if SGMII autonegotiation is finished between MAC and PHY.
-Regards
Aniruddha
Hi Aniruddha,
Could you help explain what's the difference between 0x01 bit [2] and 0x0133 bit [12]? Why do we need to read it twice?
My customer see random link up (0x0133 bit [12] without connecting partner PHY)....
thanks
Dongbao
Hi Dongbao,
I am checking in our internal database for register 0x133 clarification. I will get back to you by Wednesday (08/12). Does customer see bit [1:0] are also changing without connecting to link partner?
-Regards
Aniruddha
Hi Dongbao,
Can you share the full register read value for 0x133 when the random link up occurs? After checking with internal database 0x133[12] is not a latch low bit so it only needs to be read once. It is a duplicate link up status register.
-Regards
Aniruddha
Hi Aniruddha,
Thanks for your feedback.
I am working with Virkam offline to solve this issue.
Dongbao
Hi Dongbao,
Thanks for the follow-up. I will close the thread here since this issue is being debugged offline.
-Regards
Aniruddha