This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Quote# QB9B7B4 - Ethernet PHY/Transceiver for CPU with RGMII interface supporting up to 1000Mb/s

Other Parts Discussed in Thread: DP83869

Hello,

can you possibly advise on the following customer question regarding an Ethernet PHY/ transceiver, which the customer is looking for?

The customer mentioned: 

I actually want to connect two cpu's (iMX8 from NXP) with the Ethernet protocol on the same pcb. My thoughts so far are to connect them in the following manner:

RGMII (CPU1) PHY magnetics pcb traces magnetics PHY RGMII (CPU2)

I would like to do it without the RJ-45 jacks, since the application should be as lightweight as possible.

Can you possibly advise a suitable transceiver?

Thank you very much.

Best regards

Adnan