Part Number: LMH1228
Hi team,
1. In the below condition, is the adaptive EQ mode recommended rather than manual mode?
Datarate: 12Gbps
Trace length: 0 ~ 20 inch
2. Datasheet says EQ can compensate up to 20 inch of trace length. Can this device support more than 20 inch of trace length?
3. Could you give me the recommended EQ value for 10inch and 30inch trace in manual EQ setting?
Regards,
Saito