Part Number: PCA9306
DHello,
Regarding to PCA9306, my customer is asking a question.
.(Question)
Can this device use for HDMI DCC bus level shifter(5V<->3V)?
Regards,
Tao_2199
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Tao,
This device can be used as a level shifter at those voltages but just to be clear, this device does not buffer the capacitance of the cable side. You would need a I2C buffer/repeater (many of which in our portfolio have level shifting capability).
Thanks,
-Bobby