Part Number: DS8921
I have a second occurrence where when the interface is powered up before Vcc of the device, the device is damaged.
The design is one board with DS8921 Xcvr and the controller would be either NI PC card or in the latest case another DS8921 Xcvr.
I have point to point controller to single slave using as simple differential signal drive (no high speed comm).
How do I prevent and why isn't it designed to withstand these cases?