Part Number: TCA9803
Other Parts Discussed in Thread: TCA9517
TI Friends & Family,
One of our customers has a unique application for the TCA9803 where they are transitioning from the older TCA9517 for longevity and cost reasons. However, they need further information regarding the device datasheet specifications, particularly the current SINK spec.
The datasheet clearly identifies a current source spec (~3mA) and other forum posts suggests the current SINK spec is similar (although the TCA9517 was higher).
The question is, what is the official (or unofficial) Current SINK spec for the '9803 and also is there a difference between Sides A and B of the device which would also be applicable in this case?
Thanks for any input you can provide in advance.
Regards,
Chris