Part Number: DP83869HM
May I directly connect the DP83869HM to the Intel i210 without transformers? This is an embedded system, so the connection is not exposed and is contained on a single board.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83869HM
May I directly connect the DP83869HM to the Intel i210 without transformers? This is an embedded system, so the connection is not exposed and is contained on a single board.
Hi Wesley,
Direct electrical connection between Ethernet PHYs is not recommended. There needs to be some sort of isolation. Transformer based isolation is most common method. You can also try using capacitive isolation by adding AC coupling capacitors on the MDI lines going from one PHY to another, but you will need to perform system level testing to make sure that it is working well in your application.
-Regards
Aniruddha
Hi Wesley,
DP838669HM has voltage mode line drivers. You do not need to connect biasing resistors on the MDI pins.
Dual transformer connection is what we have characterized since that is the most common use case. However, single transformer/capacitor can also work but I will recommend you to run your own system level test to ensure proper operation.
-Regards
Aniruddha