Part Number: ONET4291VA
Is it a problem to use the output stage of DOUT +/DOUT- of the ONET 4291 VA with no load (open state)? (IMOD=15mA)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ONET4291VA
Is it a problem to use the output stage of DOUT +/DOUT- of the ONET 4291 VA with no load (open state)? (IMOD=15mA)
Greetings,
MOD + and MOD- have no termination of 50 ohms.
Will the MOD + and MOD - terminals be damaged?
thanks
Greetings,
Device has not been characterized under this condition. So i cannot be 100% sure. Having said this, given there is no current return path, i do not expect terminal to be damaged.
Regards,, Nasser