Part Number: TLK2711-SP
Hi,
What is the allowed maximum trace length for the each group TXD0/TXD15, RXD0/RXD15, DINRXP/N and DOUTTXP/N on PCB?
What is the length matching tolerance for the above signals?
Please let me know.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLK2711-SP
Hi,
What is the allowed maximum trace length for the each group TXD0/TXD15, RXD0/RXD15, DINRXP/N and DOUTTXP/N on PCB?
What is the length matching tolerance for the above signals?
Please let me know.
For guidance on the high-speed serial interface maximum length you may reference the previous E2E post per link below.
I could not track down length matching tolerance data for the 16-bit parallel interface. I would recommend to reference the IEEE GMII timing requirements as a guideline.
Cordially,
Rodrigo Natal
HSSC Applications Engineer
Thank you for the information.
But i am not cleared about what is the maximum allowed length for parallel data lines?
Can you please help?
Hi Anand,
The maximum distance of the parallel traces will be determined by the trace attenuation. Typically, the parallel interface can handle >1dB of loss at 125MHz (which is the maximum clock frequency for the parallel interface. For a typical 7 mil FR4 microstrip 1dB of loss at 125 MHz will take ~ 13 inches of trace. If the traces are wider or the clock frequency is lower, it will take a longer trace length to result in 1 dB of loss.
Regards,
Lee