Hello,
I'm using DP83867 as Phy IC for IMX6(Freescale),The IMX6(Freescale) can't deal with a full 1000M throughput,and the limitation is at the data link layer inside IMX6,This problem troubles me a lot.if the DP83867 running at 100M mode or some lower speed mode,This problem can be solved.
The DP83867 may link with PC directly,or link with some 1000M IP switches,The Auto Negotiation Must be done,PC or IP switches don't changed any parameters.
Is there anyway to disable 1000M mode for DP83867 by setting some registers or cutting some lines on PCB?
Best regardes
Tom