This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB320: IDpin's configuration.

Guru 11455 points

Part Number: TUSB320
Other Parts Discussed in Thread: TPS66020,

Hi team.

I'd like to configure TUSB320 and TPS66020.

I have a question about the IDpin's configuration for TUSB320.

Is the ID pin asserted Low when the DFP or the DRP is connected?
I care if it works well When TPS66020 connecting IDpin to EN.
EN1's configuration is bellow.
*EN0 is fixed high.

High : Source pass
Low : Sink pass

Sincerely.
Kengo.