Part Number: DS90UB914A-Q1
Hello,
Let me confirm about below.
Q1. According to datasheet of DS90UB914A, there is following description.
* Differential Internal Termination Resistance
Is single end spec defined as internal termination resistance value as well ?
(Since there is no description about "internal" in parameter description "Single-ended Termination Resistance", so I asked just in case.)
Q2. According to datasheet, user can change termination resistor value from add 0x26[3:2].
I believe that datasheet termination spec is defined as "Typ 50ohm(resistor value is 0x00)", however I would like you to confirm range of other resistors.
Are other resistors characterization as +/-20% as well ?
(Ex, In case of "0x01"(47.4ohm), I assume max value is 56.88ohm(47.4ohm + 20%) and min value is 37.92ohm(47.4ohm - 20%))
Best Regards,