This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25833-Q1: DCP auto mode

Guru 29720 points

Part Number: TPS25833-Q1

Hi Team,

My customer considers using TPS25833-Q1 and asked the following question.

I understand TPS25833-Q1 can detect shorted or divider 3 or 1.2V-mode automatically in DCP auto mode.
Is there any material (application note etc.) that shows how to detect appropriate charging schemes?
The datasheet doesn't show the detail process.

Best Regards,
Yaita

  • Hi Yaita ,

    We don't have the detailed app note for this DCP auto mode.

    The TPS25833-Q1 will stay at divider 3 mode (DP/M=2.7V) when no device attached.  If the apple device attached then it can identify this is the divier 3 port and drink suitable current. if the samsung device attached it will sink the current in DP/M then it will trigger the TPS25833-Q1 going into the 1.2V mode during this mode. The device DP/M=1.2V and samsung device will sink the suitable current. If the attached device is not apple and samsung, the TPS25833 will short the DP/M which broadcast this is the DCP port and the phone will sink the suitable current. 

    So,different attached phone will trigger the different charging mode in the TPS25833-Q1.