HI team,
My customer is asking if our 936 can configure to output only D3P/N, D2P/N paired with CLK1P/N? Current they only use one camera at input port0.
If yes, could you kindly help with a detailed configuration?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI team,
My customer is asking if our 936 can configure to output only D3P/N, D2P/N paired with CLK1P/N? Current they only use one camera at input port0.
If yes, could you kindly help with a detailed configuration?
Thanks
Hello,
I believe the best way to do this would be with the CSI replicate mode found in the datasheet under section 7.4.22. Using this you can recreate the data on lanes 0 and 1 to be exactly the same as on lanes 2 and 3. When configuring the 936 be sure to set only 2 data lanes be used in the CSI_CTL register and set the CSI_REPLICATE but in FWD_CTL2 register.
Regards,
Nick