Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987
Hi,
I'm seeing an issue when TPS65987 loads the patchset+profile from "Region 1". It seems to always return wrong "Version (Reg. 0x0F)", as it always returns 0xF7071000, instead of 0xF7071008 as it should. When the patchset is loaded from "Region 0" the Version (Reg. 0x0F) correctly returns 0xF7071008.
Interestingly the custom profile is not affected and I'm able to properly negotiate custom PDO but my fear is that I will see other differences if indeed the latest TI Patch 0xF7071008 is not working with its fixes/modifications.
As a possible hint, looking through binary I see only 2 places that contain " 0xF707", one in the beginning of the Region area contains correct "0xF7071008"
but few hundred bytes lower there's a "0xF7071000", maybe that's something, or perhaps just a weird coincidence.
Could you please help clarify what are the consequences of the version coming back the older patch 0xF7071000?
Thanks,
Ilya