Part Number: TMDS181
Hi team
In schematic checklist of this device, it is connected by AC-coupling in figure.1.
I think this device supports DC-coupled input.
Is it possible for this device AC-couple connect?
best regards
teritama
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDS181
Hi team
In schematic checklist of this device, it is connected by AC-coupling in figure.1.
I think this device supports DC-coupled input.
Is it possible for this device AC-couple connect?
best regards
teritama
Teritama
Figure 1 in the TMDS181 schematic checklist is for interfacing the TMDS181 DC-coupled output to an input that requires to be AC-coupled.
The TMDS181 input can be AC-coupled but not recommended. In the case of AC coupling the TMDS181 input, the input voltage would then become 3.3V + Vswing so the input voltage exceed TMDS181 absolute spec.
For AC-coupled input, I would recommend DP158 or DP159.
Thanks
David