Part Number: DP83TC811S-Q1
Hi Sir,
Now our design PHY and RJ45 are placed at two separated board.
What is the magnetics placement rule closing to either PHY or RJ45?
And what is the routing length constraint in DP83TC811S?
thanks.
Alpha
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83TC811S-Q1
Hi Sir,
Now our design PHY and RJ45 are placed at two separated board.
What is the magnetics placement rule closing to either PHY or RJ45?
And what is the routing length constraint in DP83TC811S?
thanks.
Alpha
Hi Alpha,
For automotive phy 811 connector should be matenet connectors and not RJ45. We recommend the following because there are stringent phy level IEEE specs of mode conversion, return-loss etc and also these are helpful to meet automotive EMC/EMI requirements :
1. the connector and phy to be on the same board
2. mdi traces : matched 100 ohms differential routing
3. mdi traces : burried (if possible)
Also please refer to these app-notes for further layout guidelines :