Part Number: TS3USB221
Hi,
I want to use this device for I2C signal path switching.
Is it possible?
If possible, should I connect the I2C Pull-Up resistor to only one terminal?
I would like to use it with the following configuration.
D+/D-: Pull-up not connected
D1+/D1-:Pull-up connected (1.2V)
D2+/D2-:Pull-up connected (3.3V)
(VCC = 3.3V)
Best regards,
Ikeda