Part Number: TUSB9261-Q1
Other Parts Discussed in Thread: TUSB9261
Hi Team,
I have a question about maximum ratings.
The maximum rated voltage of USB2.0 DP/DM terminal is -0.3V to 3.8V.
Is this independent of the power supply voltage level of the TUSB9261?
For example, will the maximum rating of DP/DM terminal be -0.3V to 3.8V even when VDD33/VDDA33/VDD is off (0V) ?
Best regards,