Part Number: DS90UH948-Q1
Hi Team,
I read the UH948 datasheet to understand the DGPIO setting. Could you let me know if I have any misunderstand in below points.
1. DGPIO only could use in 2-lane FPD link.
2. GPIO and DGPIO are pair setting. I mean that GPIO3 direction setting should be the same as D_GPIO3.
3. 7.3.9.1 table2 means the direction setting of GPIO/D_GPIO. If I set (947)0x0D[3:0]=0x3 and (948)0x1D[3:0]=0x5, does it mean that the 947 D_GPIO0 is an input and D_GPIO1 is an output?
4. If I set (947)0x0D[3:0]=0x3 and (948)0x1D[3:0]=0x5, And I use hardware to set 947's D_GPIO0 high and 948's D_GPIO0 will follow the 947 D_GPIO0, is it right?
5. Instead of use hardware method to set the pin high or low, could we use the register to set input state and then output follow the input?
6. Do we have register to know the D_GPIO output state?(ex. forward 947 to 948, if 947D_GPIO0 is high, 948D_GPIO0 will be high, do we have register to know the 947D_GPIO0 and 948D_GPIO0 state?)
Thank you for your support.
Regard,
Roy