Part Number: ONET8501V
If there is no load connected to the MOD+/MOD- terminals, or if a high impedance load is connected to the MOD+/MOD- terminals and the maximum output voltage level (IMod=24mA) is set, is there any problem or danger?
For example, does the output amplitude of the Main Driver exceed the rating, causing problems such as pin destruction?