Part Number: LMH0324
Dear Sir or Madam,
I would like to operate the LMH0324 without any programming. The operation I like to achieve is, that a 1,485 Gbps HD-SDI Signal is simply passing through the device, so that I can handle it on the 100 Ohm differential side of the device. According to the online data sheet this should be possible.
Currently I´m not sure, what to do with the following Pins:
- SS-N_ADDR0
- SCK_SCL
- MOSI_SDA
- MISO_ADDR1
- MODE_SEL
Can they simply be left floating or should these be tied to GND, VDDIO....
Thanks in advance,
BR, Martin