Part Number: THVD2450
Hi,
To save space and upgrade robustness against machine wiring faults, I am considering upgrading from
SN65HVD485EDR (in SOIC8)
to
THVD2450 (in VSSOP8)
in this new version of the circuit board.
- Is THVD2450 the best choice for industrial environments? (were 30V can accidentally be shorted to RS-485 data line)
- Is there any advantage to THVD2450 in the larger SOIC8 vs. VSSOP8?
- Do manufacturers have trouble with the SON package floating off the pads?
- Which package has the highest quantity per year demand?
Thank you for your help.
Best,
~Alicia