This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB2036: 48MHz frequency tolerance...

Part Number: TUSB2036

In the related E2E post, it was recommended the 48MHz OSC have a frequency tolerance of 50ppm. The customer has selected a device where, after 10 years, the ppm degrades to ±70ppm.

This goes beyond the ±50ppm recommendation, but is this acceptable? Any concerns?

OSC: KC2520B-C1
P
N: KC2520B48.0000C1GEBC

Regards,

Darren