This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ONET4201LD: MOD+/MOD- terminals

Part Number: ONET4201LD


If there is no load connected to the MOD+/MOD- terminals, or if a high impedance load is connected to the MOD+/MOD- terminals and the maximum output voltage level (IMod=80mA) is set, is there any problem or danger?

For example, does the output amplitude of the Main Driver exceed the rating, causing problems such as pin destruction?