Part Number: TCA6416A
Other Parts Discussed in Thread: SN74CB3T3245, TCA9555, TCA9535
Hi Support Team,
In our application (battery powered), we have multiple boards, the host μC resides on board A.
on Board B, I have I/O lines for status monitoring and control and I was looking at TCA6416A.
Now, if I understand correctly, VCCI can be powered ON while VCCP is OFF, this keeps the TCA6416A in RESET state
#1 is it possible to power VCCP while VCCI is NOT powered?
There is a scenario where board B is powered UP meanwhile board A and μC is powered OFF, and the concern here is power back feeding to the μC.
For protection, my first thought is to use a switch, i.e. SN74CB3T3245 in front of the TCA6416A
#2 what is correct configuration for unused pins for lowest current consumption?
Configure as INPUT and
a) tie HI directly
b) tie LO directly
c) tie HI with pull-up
d) tie LO with pull-down
leave floating and configure as OUTPUT HI?
leave floating and configure as OUTPUT LO?
#3 can you please explain main difference between TCA6416A and TCA9535/TCA9555 (with internal pull-ups) ?
Best,
AJ
There is a scenario where board B is powered UP meanwhile board A and μC is powered OFF, and the concern here is power back feeding to the μC.
For protection, my first thought is to use a switch, i.e. SN74CB3T3245 in front of the TCA6416A
μC