Part Number: SN65HVD10
Hi, could anyone help me with decoding date codes to determine when the parts were produced?
marking is VP10Q which is SN65HVD10QD
remaining markings:
part 1: 4CM A7HE
part 2: 59M AHE1
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sergio,
The date of assembly is given in the three-character code on the second row of top-side markings. The first character represents the year (e.g., "4" = 2014) and the second character represents the month ("1" = January, "2" = February, ..., "A" = October, "B" = November, and "C" = December). The last character is a code for the assembly site used (in this case "M" represents TI Mexico).
Max
Sergio,
The third line is a unique lot trace code. You can't get any meaning from the characters themselves, but we could use them if needed to track down more info on the specific assembly lot the unit originated from. If you wanted I could check with our component quality team to look these two up to see if we can give a specific year. Otherwise you would either need to make a guess as to whether they were 2004 or 2014 based on when they were purchased or refer to the label information (if you still have access to this, I believe they generally write out the full year).
Max
If you could look those up, it would be great! Looks like they were put on custom reels at some point, so no markings there. I want to make sure we use the latest parts, not something which was in storage since 2004.
Thank you!