Part Number: SN65HVD235
Other Parts Discussed in Thread: SN65HVD1050
Hi team,
Customer will use both 3.3V CAN (SN65HVD235) and 5V CAN (SN65HVD1050) in the same CAN bus.
- Could both 3.3V CAN and 5.0V CAN use in the same CAN bus ?
- If yes, are there any reference design, application report or material that describes it is no problem as CAN standards ?
- Should customer the ratio between 5V CAN and 3.3V CAN in the same CAN node ?
If yes, what should customer think about ?
e.g.
Are there any issue if there are five nodes at 5V CAN and 2 nodes at 3.3V CAN ?
Thank you and best regards,
Michiaki