Part Number: SN75176B
Other Parts Discussed in Thread: THVD1550, THVD1500
Hi Team,
My customer reported an issue that the R PIN of 75176 received an unexpected signal:
The R PIN of SN75176 received an unexpected signal with differentiated signal is 0 while the load (motor driver) is active, but the R PIN stayed as normal without load(motor driver is de-active). The 2 RS485 nodes are connected by a 25m cable connected to the bus;
It’s obvious affected by the noise, but the differentiated signal kept as normal, could you kindly give comments on 2 items?
-
Reason analysis
-
Solution recommended
More details like schematic and test waveform could be found as attached file: SN75176 received unexpected signal when AB differentiated signal is 0.docx
Expect for your reply, thanks.
Best Regards
Benjamin