Part Number: XIO2001
6.12.2 in the Datasheet states PCIR needs to be powered-down before the +V_IO 3.3V rails.
In the EVM user's guide, PCIR is connected to the 3.3V supply via a 1kΩ resistor and 0Ω resistor.
In this case, if the 3.3V supply was powered down, the slight charge on the 0.1uF capacitor would mean the PCIR voltage would actually power down ever so slightly after the 3.3V supply was powered down...
Could I get some clarification on the power-down sequence, with emphasis on PCIR when used at 3.3V?