Part Number: DS90UB954-Q1
Hi Team
I got a problem while ESD contact test,FPD Link get fail ,no video show up.(maybe some radiation issue combined like this)
The system is 954 connect to 953 through BNC connector and coaxial cable with POC 24Vdc (BNC is DIP type)
I'm understand good shielding is necessary ,so the trace between UB954 pin and BNC connector ,routing on an inner layer is better than routing on the layer same with UB954 ?
In datasheet ,Layout example shows Differential Signal Traces routing on inner layer ,and POC example routing on outer layer
I wonder know is single end trace can routing like differential signal on inner layer for reduce ESD impact reason ? (UD954 is near by BNC connetor)