Part Number: DS90UB936-Q1
Hi team,
My customer is going to use 24MHz reference clock instead of 25MHz crystal.
I know the forward channel data rate and CSI2 output are affected this slower reference clock and, the datasheet 7.4.4 REFCLK section describes "back channel rate, I2C timers, CSI-2 datarate, FrameSync signal parameters, and other timing critical internal circuitry" are works on the REFCLK but need more detail.
Could you list up "ALL" parameters which is affected from using 24MHz clock instead of 25MHz for example GPIO maximum frequency, AEQ relock time, I2C watchdog and high/low time or so?
Best Regards,