Part Number: DS90UB960-Q1
hi teams:
we are using the 960+935+4 sensors.The sensor output is the same pixel 1920*1080.
we use 960 two ports output data to two csi2 of cpu.
sensorA----------| -------------960 csi2 port 0
sensorB----------|
sensorC----------|--------------960 csi2 port 1
sensorD----------|
4 sensors can be opened separatly, but can not be open at the same time occasionally.
when we using the 960+933+4 sensors, and the same pixel, there is no such phenomenon,
the 960 reg configuration is following, Are there any other inaccuracies? Please look at this problem for me, Thanks.
ti960_write_reg(client, 0x4c, 0x01);
ti960_write_reg(client, 0x58, 0x5e);
ti960_write_reg(client, 0x5c, 0x30);
ti960_write_reg(client, 0x5d, 0xda);
ti960_write_reg(client, 0x65, 0xba);
ti960_write_reg(client, 0x70, 0x1e);
//"*** RX1 VC=1 ***"
ti960_write_reg(client, 0x4c, 0x12);
ti960_write_reg(client, 0x58, 0x5e);
ti960_write_reg(client, 0x5c, 0x32);
ti960_write_reg(client, 0x5d, 0xda);
ti960_write_reg(client, 0x65, 0xbc);
ti960_write_reg(client, 0xb0, 0x1c);
ti960_write_reg(client, 0x70, 0x5e);
ti960_write_reg(client, 0x72, 0x55);
msleep(5);
ti960_write_reg(client, 0x4c, 0x24);
ti960_write_reg(client, 0x58, 0x5e);
ti960_write_reg(client, 0x5c, 0x40);
ti960_write_reg(client, 0x5d, 0xda);
ti960_write_reg(client, 0x65, 0xbe);
ti960_write_reg(client, 0xb0, 0x1c);
ti960_write_reg(client, 0x70, 0x9e);
ti960_write_reg(client, 0x72, 0xAA);
msleep(5);
//"*** RX1 VC=3 ***"
ti960_write_reg(client, 0x4c, 0x38);
ti960_write_reg(client, 0x58, 0x5e);
ti960_write_reg(client, 0x5c, 0x42);
ti960_write_reg(client, 0x5d, 0xda);
ti960_write_reg(client, 0x65, 0xc0);
ti960_write_reg(client, 0xb0, 0x1c);
ti960_write_reg(client, 0x70, 0xde);
ti960_write_reg(client, 0x72, 0xff);
msleep(5);
//"CSI_PORT_SEL"
ti960_write_reg(client, 0x32, 0x01);
ti960_write_reg(client, 0x33, 0x03);
ti960_write_reg(client, 0x32, 0x13);
ti960_write_reg(client, 0x33, 0x03);
ti960_write_reg(client, 0x20, 0xFC);
ti960_write_reg(client, 0x20, 0x0C);