Part Number: TCAN332
Hello,
I want to know is this IC supports ISO 15765 protocol as in the datasheet only one protocol is mentioned but nothing mentioned about others. Can someone help me on this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jay,
ISO 15765 is a transport layer protocol that is defined in the controller of the CAN network. The controller communicates with the bus through the CAN transceiver, and the TCAN332 is a CAN transceiver. The transceiver is agnostic to the protocol beyond data rate limitations, and since the TCAN332G can work up to 5Mbps, this should work fine.
Please let me know if you have any other questions.
Regards,