Part Number: MAX3238
We have a product that we have been selling for about a decade that uses a MAX3238C. Recently we had a production run and 3 devices failed in the field. One failed after a few days, another failed after a few weeks, and the third was installed back in December 2019.
Investigation into the issue discovered that the MAX3238C chip failed. Failure caused all the outputs to be less than one volt. The charge pump was oscillating but only also under a volt. Supply voltage was +5V. C1 = 0.22 uF and C2 – 4 were 1 uF. Force On and Force Off were both connected to +5V.
As this design has been in the field for almost a decade, and we have sold over 500, we don’t believe the issue is a design flaw.
We also did not uncover any external events that may have caused the failure. Each failure came from a different location. There was nothing different in the installation than any of installations done in the past. These are the first failures we have seen of the MAX3238C.
According to our records, the chips used in the past were also TI MAX3238C.
It occurred to us there may be a problem with the chips themselves. Possibly a CFSI issue. The markings on the 3 chips are all the same:
Top Line: (TI Logo) 52CYSEKC4, with the C4 underlined
Second Line: MAX3238C
Has anyone had failures with these chips?
Any assistance would be appreciated